Other Parts Discussed in Thread: STRIKE
For the second time during debugging it seems the DRV8308 5 Volts regulator burned out.
It seems it burns out at power up. The enable pin is pulled-up to VM with a 10K resistor and 5V zener to gnd.
At the 5 volts output there is a 0.1uF cap and a 10uF to supply the halls and microcontroller.
The Vsw output is not in use.
Total Vreg consumption is <20mA.
If I connect now the board to the power supply the current draw is only 3mA and there is no voltage even on Vint pin.
The VM pin has 2 10uF/35 ceramic capacitors.
Any clue?
Gian Paolo