This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8876N: Charge Pump Undervoltage Lockout

Part Number: DRV8876N

Hello;

I've set up a circuit using the DRV8876N Motor Driver, but upon testing have found that the chip is not operating and the fault indicator is showing a fault condition.

According to the data sheet, the fault indicator will show a fault condition when VCP pin is less than 2.25 V with respect to VM. Upon investigation I've found the VCP pin is exhibiting a sawtooth waveform from 0.8V less than VM to 0.8V more than VM. Can you please provide assistance in correcting this issue?

VM is 11.6V

VM to GND bypass capacitor - Parallel 0.1uF 100V C0G and 10uF 25V X5R ceramic capacitors

VCP to VM charge pump storage capacitor - 0.1uF 100V C0G ceramic capacitor

Charge pump flying capacitor (connecting CPH to CPL)  - 0.022uF C0G ceramic capacitor

Thanks

Jeremy