I have the exact same issue as detailed is this post: https://e2e.ti.com/support/motor-drivers/f/motor-drivers-forum/549549/lm629-pin-13-pwm-mag-and-pin-11-pwm-sign-issues?tisearch=e2e-sitesearch&keymatch=LM629#
When power is introduced to the circuit there is a chance that the LM629M-8 will output some signal on the SIGN/MAG pins before our microcontroller can reset it and initialise the device correctly. When this happens it causing the motor to spin very fast until the micro stops it. As in the linked post the PWM duty is at one extreme but in our case is high (>90%). Therefore the motor spins as if direct DC was applied.
We have tried fitting a pulldown to the RST pin of LM629 to hold it in reset whilst the micro is doing it POR (power on reset) but this had no effect. Is there a way to ensure that LM629 does not output any motor signal (i.e. keep SIGN & MAG low) during POR?
Regards,
Jamie