Other Parts Discussed in Thread: DRV8873, LMD18200
I redesigned a pcb for my client who used the THT IC LMD18200T for driving his motor.
The redesigned board has now the DRV8873-Q1 chip, but when I PWM the inputs like 12% ON to slowly drive the brushed geared motor, I'm basically lost all torque.
I tried PWM frequenties between 60Hz to 300kHz, but no results.
I was actually surprised to see that the PWM signals are passed on to the OUT pins, while the LMD18200T measures a continuous voltage output.
Can the DRV8873-Q1 operates the same way PWM in and variable but continuous voltage out?
I'm sure the torque loss is caused by PWM pulsing the DC brushed motor.
Or what other SMD chip would you recommend?