Hello,
I want to use the LMG1210 with a non-symmetrical power supply as shown in the attached figure. As I understood reading a related post, in this setup, is it necessary to supply two isolated 5V DCDCs to HB-HS and VDD-VSS? Also, how should I connect the heatsink pads? both to GND as shown in the figure, or connected to HS and VSS to each thermal pad? And finally, is it correct to remove the boostrap diode D1?
Is there anything else I need to consider?
Thanks in advance.