Other Parts Discussed in Thread: LMV431
Hello,
I am trying to use the LM5117 in CC/CV mode to charge a 10 cell lithium ion battery pack. In order to do this, I intend to configure the LM5117 for a constant current of 2A with an output voltage of 42V once the battery enters saturation charge.
I used application note SNVA829 to help with this, however have gotten stuck in selecting a precision voltage reference as the LMV431 only goes up to 30V. I short search for alternatives didn't yield any results supporting a high enough voltage.
My current thoughts are to perhaps use a zener(s) (e.g. 20V zener voltage) in series with the LMV431 to reduce the reference voltage requirement.
Would this work? But also am I going in the right direction by using the LM5117 for this purpose in the first place?
Cheers,
K