Dear sir:
When using bq25792 to realize 1-cell battery charging, the following problems appear, please help to confirm the cause,thank you !
1.The charging current of bq25792 is set at 1.5A. When the battery is charged to about 3.1V, the charging current is less than 100mA, and the charging current is unstable. The vsys is only about 3.8V
The measured waveforms are as follows:
2.Replace the 1pcs battery with a voltage of about 4.1V for charging confirmation. The measured waveforms are as follows
VSYS=4.2V,Ibat=260mA
3.Recharge the 3.1v battery and confirm that the charging current can reach 1.5A,VSYS=4.2V,Ibat=1.46A
The above conditions of 2pcs battery are detected, and the register settings are as follows:
REG00 0x04 |
REG01 0x1A4 |
REG03 0x96 |
REG05 0x2F |
REG06 0x12C |
REG08 0xC3 |
REG09 0x05 |
REG0A 0x23 |
REG0B 0xDC |
REG0D 0xBB |
REG0E 0x39 |
REG0F 0x22 |
REG10 0x80 |
REG13 0x01 |
REG14 0x1E |
REG17 0x7A |
REG18 0x14 |
The circuit diagram is as follows:
Please help to confirm the cause of the defect,Thank you !