Other Parts Discussed in Thread: UCC27322, UCC27524
Hallo all
I have a question about propagation delay. I find it difficult to estimate the propagation delay of this device.
When I compare UCC27322 with UCC27524A1, the propagation delays are defined differently.
The UCC27322 is measured over the entire temperature range and the start and end points are also defined as 20% - 80%.
The UCC27524 is measured at room temperature, and the start and end points are also defined differently.
At first glance, the UCC27524 looks much, much better. How can the two drivers be assessed in relation to each other and under the same conditions?
We want to operate a MOSFET between 70-150kHz, so the delay time variance should be as low as possible so that we can compensate for it.
We want to resolve the PWM signal to 1-2%.
Best regards
Olaf