Hello,
We are looking to build a system with BQ24295 and here are some design questions:
- The Vin is from a DC-DC converter at 4.4V and we want the input current limit to be 3A. From the datasheet it isn't clear what to do with D+/D- pins when not providing power from a USB connector. In this specific case how to create a detection of charging port with 3A input current limit so that this value is written to REG0[2:0] on powering on input side?
- Once REG0[2:0] is set to 3A limit, the actual limit is set as per ILIM pin's resistor, right?
-The battery would need slow charging to prolong its life, so max charging current needs to be 300 mA. This means with 20% as max ripple current of inductor, its 60 mA. Using this value if we calculate the inductance needed, its more than the 2.2uH recommended. So how do we go about this?
-There is no load on PMID as there is no requirement of OTG. As I understand from another thread in this case the min capacitance needed at PMID is 8.2 uF. Please confirm this.
- If there is no need for temperature sensor at TS pin, how can this pin be setup for no error?
Thanks, Prithvi