Greetings,
I have a problem with large output voltage ripple in any L-C combination. ( Load 0.6 - 2 A)
If i change the input voltage to 12V, then the output ripple is minimal with the same configuration.
What could be the problem?
Example:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings,
Hi, Igor
For high conversion ratio: 24Vin to 1Vout, it need large Cout to make loop stable.
Suggest changing L1=1.5uH, and enlarge Cout bigger than 300uF, then redo the simulation.