Hi
There are then evaluated using the client BQ25306, input 12V, 1.5A for setting 2cell lithium battery. According to the specification, the charging current will stop if the charging current is lower than 0.15A. Customers are worried that the battery voltage will be low at this time. Is there any way to charge the battery voltage to a higher voltage?
Thanks you