Other Parts Discussed in Thread: TPS54361-Q1, TPS54561, TPS54361
Hi,
We would like to use TPS54561-Q1 in our new design. I'm not able get a solution using TPS54561-Q1 when I try to create one using Webench with input EMI filter added. But it's generating design using TPS54561-Q1 if I'm not adding input EMI filter.
Input:DC 8 V - 60 V
Output:5 V at 3.5 A
Frequency : 800 kHz
Is that good enough to use the design based on TPS54361-Q1 with EMI filter and use TPS54561-Q1 instead of TPS54361-Q1