Hi,
Good day.
Our customer is using the LMR36506-Q1 and they have this inquiry:
I would like to know what the quiescent current draw is for the LMR36506-Q1 when in standby mode (i.e., VIN less than turn-on voltage) with a turn-on voltage set to 5.5 Volts via the resistor divider at the EN pin.
I see that the datasheet claims 0.5µA current in shutdown and it shows plots of current draw when active, but I cannot find details of current draw during the standby mode that occurs between those two states.
I hope you could help us with this. Thank you.
Regards,
Cedrick