Other Parts Discussed in Thread: BQSTUDIO
Hi, guys! We developed our 13S BMS to the point, where first 500 pcs must go to production.
During the production phase we also need to program parameters via OTP, which we do now manual using bqStudio (Data Memory > Import ...) .
However, we would now like to make it easier for mass production: does TI offers some command line tools or something for BQ mass production programming, so we could make it "one click" programming:
> Checking for the IC presence on I2C
> Writing parameters from file
> Writing current parameters, that are not imported from file (CC Gain, Capacity Gain)
> OTP check
> OTP programming
Best regards,
Gregor MACEK
p.s. There is a bug in bqStudio application (1.3.104): after importing file .gg.csv, Cell 13 Gain and Cell 14 Gain are also changed and must be manually modified back to old values before preforming OTP. Is this fixed already?