Hello team,
1. If the load is not their battery is charging from the source but after the load is connected both PG(led) and stat(led) fluctuate and my load also fluctuate and the load is around 8W. As soon as I remove the source i.e 12V, load works fine. I am using a DC bench power supply so no issue with the source. Please check the schematic ILIM is 1k and ICHG is 667. I tried to change the ILIM value to 330 ohms. but the problem persists.