This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2961: BQ2961 - Looking for design review

Part Number: BQ2961

Hi,

I have designed a battery protection circuit for two LiPo cells and I want to ask if this circuit is fine or if there are some issues with this design.

The circuit should be optimized for low power. So I use 1 MOhms resistors for the pull-up / pull-down resistors.

Are there any issues with this circuit?