Other Parts Discussed in Thread: BQ25890H, BQ24259
Hi, team,
My customer had a design with bq25890H, but due to the heavy supply shortage. They want use put bq24295 on the PCB of bq25890H, because 24295 is pin-pin with bq25890H.
However, there are several pins have different definition. Can they only connect pin 2 for Vbus input, but leave pin24 float? Their charging current is 2A.
Can they leave pin PSEL float? Per datasheet, at power on or adaptor plug-in, bq24295 detect PSEL voltage and decide input current limit register and VBUS status register. But they can also change the current limit by software. So that won't be a problem. Right?
Besides these two questions, please suggest if we have missed something? Thanks!