This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3431-Q1: Can we keep EN pin floating to get logic low?

Part Number: TPS3431-Q1

Hi,

There are some cases in my application that the driving circuit for EN pin will become floating when I expect the EN should be logic low.

From the datasheet, EN pin is internally pulled up to VDD. Besides, I have to minimum the driving current of EN pin. 

Therefore, I am not sure if it is required to externally pulI down EN pin for stable logic low when external driving is floating. 

If an external pull down is required, please let me know the maximum allowed resistance to minimize current consumption.

Thanks.