This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25018: SW to RTN absolute max

Genius 15840 points
Part Number: LM25018

Hello,

 

My customer has a question for LM25018 absolute max, SW to RTN(100ns transient).

 

The datasheet defines its MAX value as “VIN+0.3”.

But I believe that it is almost impossible to keep this spec at the switching timing.

SLVA494A application note says over “VIN+0.3V” in a short time is acceptable.

Can this application note be applied for LM25018?

 

Regards,

Oba