This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI's taem
We want to use UC3842 as a Voltage Mode PWM.
Do RT/CT circuits need to be connected like the below picture from datasheet?
Can it be connected like the typical circuit (just using a resistor and capacitor)?
Will the voltage mode be better for avoiding entering pulse skipping when the output voltage is very small?
Thank you very much.
Hi Alvin,
I would leave the circuit as you see it in the data sheet. The idea is to completely buffer the ISENSE pin so that only the divided down, buffered RT/CT RAMP is fed into ISENSE.
Steve M
Hi,
The circuit you've shown in the red box is a current source. The 1N4148 compensates the Vbe change with temperature, so the current is “constant” over temperature. A current source charging the CT capacitor provides a more linear RAMP at RT/CT instead of the RC time constant type waveform when you connect RT, CT directly from VREF.
Since the RT/CT RAMP is linear, the voltage mode control ramp at ISENSE is also linear. The importance of this is that your small signal gain depends on the dV/dt of the ramp. With the linear ramp, you ensure that your gain remains constant.
You can use the RC waveform if you can tolerate the changing loop gain. In practice, if your loop is slow and you have plenty of margin use the RC. If you want a little bit better performance and you push the gain bandwidth, use the current generator and the linear ramp. Your choice. Thanks for connecting through E2E.
Regards,
Steve M