Hi,
I'm using the TL431 to generate a 19V and a -10V reference rail @ 5mA.
I have 10uF of capacitance on the output but this is a ceramic capacitance with very low ESR. Looking at SLVA482A - do I also need to add some ESR? If using a ceramic capacitor, would this just be adding a series resistor between the capacitor and the cathode? What value would you recommend?
Am I right in thinking the higher the resistance, the higher the deviation in cathode voltage during transients?
Many thanks