Part Number: EMB1412
Other Parts Discussed in Thread: UCC5350
Hi Team,
Just a little clarification on the VEE rating for EMB1412. The abs max rating table shows a rating of IN_REF-VEE of 5V max. However, section 7.1 of the datasheet mentions that VEE pin supply can range from IN_REF potential to as low as 14V below Vcc. Using 14V VEE below Vcc for example would exceed the max abs max rating of IN_REF-VEE.
Our customer would wish to use it for -10V VEE operations. Can you help us clarify which would be the correct recommended working conditions for VEE?
Thanks in advance!
Kind Regards,
Jejomar