Hello,
What values are recommended for the VBUS diode and the PFET when using the BQ25302 in an application with an external power path (2A maximum)?
Thank you and regards,
Alfred
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What values are recommended for the VBUS diode and the PFET when using the BQ25302 in an application with an external power path (2A maximum)?
Thank you and regards,
Alfred
Hi Alfred,
It is up to the designer as this is a reference circuit. Keep in mind values of Qg, RDSon, drain current rating for the PFET. Rate diode for forward current > gate drive current required to charge the the Ciss of the PFET.