This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is trying access the time from "Power ON" using an external DC adapter to I2C ready?
How long does PG requires to go low after power ON?
Do we have to wait for PG going low before accessing I2C?
Currently we are seeing about 300ms from the time DC adapter applied to PG going low. Is that normal? Do we have a spec on that?
Thanks!
Christina
Christina,
1. It depends on the input source type. /PG goes low after input source type detection is completed. Please refer to 8.3.3 Power Up from Input Source for the details.
2. No, I2C will be ready shortly after POR. Please refer to 8.3.1 Power-On-Reset (POR) on the d/s.
3. Please refer to Fig.30 on the d/s for an example.
Thanks,
Ning.