May I know what is the Internal FET of the body-diode forward voltage? We don't see it in the datasheet.
BR, Gary
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
May I know what is the Internal FET of the body-diode forward voltage? We don't see it in the datasheet.
BR, Gary
Hi Gary,
By internal FET body-diode forward voltage, are you referring to the high side FET? The high side FET should not be forward biased which will result in current flowing from SW to VIN through the high-side body diode.
If you are wondering about the catch diode forward voltage, assuming you are using the PDS760 schottky diode recommended in the datasheet, the typical forward voltage is 0.52V at 5A.
Regards,
Jimmy
Hi Gary,
I would need to get in contact with the previous systems engineer responsible for this device since this is not something that is specified in the datasheet as you've mentioned.
When I get more information on this, I'll let you know.
Regards,
Jimmy