I trying to write a register 0x405 but i send the slave address 0x48
but i see
in the data
need to change the address according the page we need
according to this the slave address should change to 0x4c?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I trying to write a register 0x405 but i send the slave address 0x48
but i see
in the data
need to change the address according the page we need
according to this the slave address should change to 0x4c?
Hi Santiago,
What is the device orderable part number (OPN) you are trying to communicate? The default I2C1_ID is 0x48 as described in datasheet but per OPN the NVM can be different and also the address.
What comes to the WD register those are addressed per I2C2_ID which is default 0x12. So if secondary I2C (GPIO2 and GPIO3) is not in use WD registers are addressed through I2C1 lines with I2C2_ID.