This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is unfamiliar with BQ25600 and have the following questions :
Questions:
Thanks
Christina
Hi,
1. Please single read REG09. REG09 keeps all the fault information from last read until the host issues a new read. In order to get the fault information at present, the host has to read REG09 for the second time. The only exception is NTC_FAULT which always reports the actual condition on the TS pin.
2. Please refer to Table 16. REG09 Field Descriptions for the details. THERM_STAT refers to Thermal Protection (8.3.10.3.1 Thermal Protection in Buck Mode). The host should monitor REG07, REG08, REG09, REG0A regularly.
3. When REG07[5]=1, the device should be in ship mode. But REG07[5]=0 does not indicate the device is not in ship mode. There's no dedicated bit indicating ship mode.
Thanks,
Ning.