This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24072T: Battery charging stopped at 4.1 V and not fully charged

Part Number: BQ24072T
Other Parts Discussed in Thread: BQ24072

Team ,

We are using BQ24072RGTR and planning to migrate to BQ24072T . In BQ24072T ,we are not using TS pin and so we used 200K Ohm and 49K Ohm as per datasheet . Even after installing these values , battery is charged. We have even alerted  those resistance but battery didn't charge. What could be the reason behind this . I have also attached schematics for your reference.BQ24072T.pdf