This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54426: ERROR(ORPSIM-15108): Subcircuit TPS54426_TRANS used by X_U1 is undefined

Part Number: TPS54426

Hi Team,

A Japanese customer has an issue on the TPS54426 Unencrypted PSpice Transient Model simulation.
He downloaded 'TPS54426 unencrypted PSS transient model package (Rev. A)' from TI HP,
and imported it to PSPICE.

He got an error.

---------------------------------------------------------------------------------------------------------------
ERROR(ORPSIM-15108): Subcircuit TPS54426_TRANS used by X_U1 is undefined

--------------------------------------------------------------------------------------------------------------
Could you please give us an advice how to deal with this error?

BTW, I gave some solution to customer, but this issue is not resolved.

Solution1.
ERROR(ORPSIM-15108): Subcircuit TPS54426_TRANS used by X_U1 is undefined

1.Select a suitable model from a vendor website
2.Change model to a suitable format
3.Open PSpice for TI and Generate Part
4.Place part in schematic
5.Set up simulation
6.Run Simulation

Kindly follow this link to view video
training.ti.com/pspice-ti-3rd-party-model-import

Further information available in this FAQ:
e2e.ti.com/.../faq-pspice-for-ti-how-do-i-import-a-3rd-party-model-into-pspice-for-ti

Solution2.
e2e.ti.com/.../ti-pspice-error-orpsim-15108-subcircuit-undefined

According to the above suggestions, delete and reconfigure the part from the schedule, and the results are the same.
During reconfiguration, there are not found in the configured libraries and information.
However, the Lib of the part appears to be set in simulation settings configuration files,
A set of environment is attached.
Could you please fix it?

TPS54426_PSPICE_TRANS_0914.zip

Thanks.