Other Parts Discussed in Thread: TPSM84624, , TPSM84424
Hi team,
i can't seem to find it in the datasheet. can you please let me know?
additionally, are there any footprint compatible modules for 6A and 8A?
Thanks,
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
The output voltage accuracy for TPSM84824 if affected by the tolerance of the external RFBT and RFBB resistors which normally adds about 2% (1% per resistor) and the internal reference which is +-1%, so on average it totals about 3%. The footprint compatible modules are TPSM84624 (6A current limit) and TPSM84424 (4A current limit).
Regards,
Eileen Hernandez