This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: use new battery cell

Part Number: BQ40Z80
Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM, EV2400

Hi,

Previously i used the 3000mAh batteries cell with BQ40z80.

Now i am using the new 4000mAh batteries. However i still see Qmax 3150mAh on the bsq.

Also, the SOC is 7% with 25.2V battery. I think the SOC is incorrect (SOC should be higher for this 25.2V). Please refer to attached figure.

What do i need to do after programming the correct chemistry ID to the BQ40Z80 (Battery ID 5441)? Do i need to do calibration or learning cycle for new battery on BQ40Z80 so that to get correct SOC?

Thanks!