Dear *,
Can you provide the part numbers for TI LDO that have a pin selectable voltage output?
We need 3.3V and 1.8V to be selected with GPIO pin.
Best Regards,
D.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Please use link for all dual output LDO's. You can select the LDO that best suits your requirements.
Regards,
Prakash L
Hello,
TPS780 is another options that provides both 1.8V and 3.3V.
https://www.ti.com/power-management/linear-regulators-ldo/products.html#p182=Programmable%20Output
Regards,
Prakash L
Hello,
I'm looking at TPS728 part number that provide 3.3 and 1.8
This is the one TPS728330180YZU, and does the TPS728330185DRV also provide 3.3 and 1.8 or 3.3 and 1.85 ?
Which part number for TPS780 provides 3.3 and 1.8 ?
Best Regards,
David.
For TPS728, you are correct about TPS728330180YZU providing required voltage.
TPS728330185DRV is 3.3V and 1.85V.
For TPS780, it will have to be the adjustable versions that uses the Vset pin.
Regards,
Prakash L