Other Parts Discussed in Thread: LM73605EVM-5V-400K, LM73605, LM5117
Dear Sir/Madam,
I am currently using an LM60440ARPKR to charge a 50 Farad 4.2 Volt supercapcaitor. It is succesfully charging this capacitor however it is taking about 50 seconds to do so. Is there anything I can do to speed up this charging time (i.e. increase in rush current).
Attached is a picture of my circuit.
- The PWR_PROT line on left of the circuit is main supply and can be anything from 8 Volts to 32 Volts.
- The output signal on the right after D39 TVS diode is fed to the supercapacitor.
Also attached is an oscilloscope plot of the supercapacitor charging.
- Blue line shows when power prot is applied (15 Volts in this case).
- Yellow line shows the voltage on the supercapacitor. Note ten seconds per horizontal division. 1 Volt per vertical division.
- for 30 seconds the supercacitor charges from 0V to 1.48V in a low current PWM mode (apx 100 to 200 mA).
- After 30 seconds the supercaitors charges upto to 4.2V in a higer current linear maner (apx 1 amp)
- Ideally I would like to charge the supercapacitor in a linear manner with a 4 amp current.
I would really appreciate any help with this. Alternatively if you can suggent a better device to do this job I would really appricatie it.