This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We have used the TPS 65133 in our design which providessplit rail power to 3x OPA4134 opamps and 1x OPA2134 audio amplifiers.
The TPS 65133 is capable of powering 3 of the 4 opamps (total of 60mA on the -5v rail with 3 opamps) but when the 4th opamp is connected, the +5V stays on but the -5V goes to 0.6V.
We haved used x7r capacitors and wire wound inductors with correct component values, however couldnt source the recommended components.
Any assistance would be appreciated.
Thank you
Hello,
Schematics/design is fairly simple for this device so I am sure yours is correct but please do send the schematics/BOM for a quick review.
Also, does the device work if you start up with 3 op amps only and than add the fourth one after the converter has ramped up as opposed to starting up into 4 op-amps? If possible, can you please also capture waveforms of the input supply, negative output and negative switch node at the time of startup? Negative converter should easily support the load currents you mentioned so it is likely some board assembly or component specification issue.
Kind Regards,
Liaqat
Hi Liaqat,
Components used:
4.7uH: LQH32CN4R7M33L - 650mA
3x 10uF: GRM21BR71A106KA73L
1x100nF: CL10B104JB8NNNC
Some tests:
Shematic:
Layout with 0.5mm trace width for power rails
5v positive and negative with no load
5V input LDO under load is OK
Negative 5V under load at 0.66V which shouldnt be possible
Any assistance would be appreciated.
Thanks,
Stefan
Hello Stefan,
I got your e-mail also on this same subject but did not get a chance to review it yet because of being very busy with some other issues. I will review and respond to your e-mail directly by tomorrow.
Kind Regards,
Liaqat