Other Parts Discussed in Thread: BQ25100, BQ24210
Hi,
When we set ICHG to 30mA, it doesn't start charging when input current below 30mA. Is there a way to start charging when input current below ICHG? For example at least with charge termination current ( %10 of ICHG -3mA ).
We are trying to charge Li-on battery from solar panels. According to sun, sometimes we may have very low input current like 1 or 3mA or sometimes we may have 30mA. In this two cases we want to charge our Li-on battery when our input current is 1 or 3mA and when our input current is 30mA. Is it possible to do that with BQ25171-Q1 or can you suggest any other IC.
Best Regards.