Hi,
I would like to simulate the LM5164-Q1 with its components for thermal analysis.
I want to understand the following points as listed.
When the ambient temperature is changed from -10 deg C to 45deg C.
1) What will be the change in output of the converter?
2) Temperature rise and steady-state temperature
3) Buck converter Output change w.r.t. external components parameter variation due to temperature change
So following are my queries
1) Will the model work for such a type of analysis? Does the model have temperature-related parameters?
2) Which software is preferred for such analysis? I am trying to use TINA but am unable to understand how to do the same?
3) Is it possible to measure temperature rise and steady-state temperature for the LM5164-Q1?
Following steps, I have taken to do the same but didn't receive any results.
Schematic Specs : Vin=48V, Vo = 12V, Io = 1A.
Observations : Vo never reaches 12V.