This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B4253-Q1: TPS7B4253 package related V-ADJ(REF)

Part Number: TPS7B4253-Q1

Hi,

I am looking for voltage tracking LDO with smallest package to track down to 1.5V. Device supply voltage is 5V and output current will be under 150mA.

TPS7B4253 should be fine, but I prefer smaller SO8 package and unfortunately in datasheet it is specified for min 2V. Internal design for this device in both packages is identical, but lower voltage is specified for bigger package to provide better cooling, or they are different internally? Device in SO8 package can work in my setup down to 1.5V or not?