This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] BQ25120A: How do I enter and exit ship-mode?

Part Number: BQ25120A


The charger can enter shipmode by:

  • To enter shipmode on the BQ25120A, the device should be operating on battery-only mode (VIN < VUVLO), and /CD and /MR must be high. Then you can:
    • Send the I2C command EN_SHIPMODE = 1 on the Status and Ship Mode Control Register (0x0).
    • Perform a button press of the MR button, if the MRREC = 1 on the Push-button Control Register (0x08).

The charger can exit shipmode by:

  • Connecting an adapter to IN (VIN > VBAT + VSLP)
  • By pressing the /MR button when VIN is not present. In this case VBAT > VBATUVLO in order for the device to exit ship-mode.