Other Parts Discussed in Thread: ADS1299
Hi, TI Support Team
A request has been received from a customer to recommend a suitable product as a PMIC for use in an EEG measurement device.
Please recommend a suitable product with the following SPEC.
From what I checked through ti.com, the TPS65070 seems to be a good fit.
If there is a more suitable product, please recommend it.
VIN : 3.3~4.2V
Vout1 : 3.3V /200mA (MCU, ADS1299, BLE)
Vout2: 3.3V/500mA (NIR 20EA)
Vout3 : 2.5V/-2.5V : 200mA (ADS1299)
Li-ion Battery charging: 5V 2A
Thnaks.
Regards,
MJ