Other Parts Discussed in Thread: UCD3138A
I've recently changed UCD3138A processor on UCD3138ACCEV149 . With the new chip, UCD3XXX Device GUI was not able to scan the device with DEVICE_ID , DEVICE CODE or PMBUS REVISION.
Only "Scan Device in ROM Mode" gave me a proper answer.
I tried to download the fimware (.x0 file) to the EVM but ı got an error at the middle of the process.
Now I am not able to connect to the EVM via JTAG or PMBUS.
These are the errors ;
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/5556.error1.png
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/8535.error2.png
What is the proper way to download firmware to the EVM and should I change the UCD3138A processor again ?