Other Parts Discussed in Thread: BQ27426
I received a GPC report, as follows:
Device / Family #1
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %
354 bq27411-G1C: 4.35V LiCoO2 1.9
3142 bq27421-G1D: 4.4V LiCoO2 5.33
128 bq27421-G1A: 4.2V LiCoO2 10.9
312 bq27421-G1B: 4.3V LiCoO2 14.49
Best generic ID 354
Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.
I cannot simply change to the bq27411 P/N as I need a system side fuel gauge.
The question is whether the bq27421-G1D variant with a 5.33% max DOD error would be "within recommended range".
Thanks,
Fred