This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2069D: Acceptable max Cout value

Genius 17295 points
Part Number: TPS2069D

Hello,

My customer has a question for Cout value of TPS2069D.

The datasheet mentioned that Cout should be min 120uF and typ 150uF for standard USB application.
Is there any limitation for max Cout value?

They want to use 150uF. But they have to use 220uF instead of 150uF because they can't get 150uF capacitor sample due to recent delivery issues.
Is it OK to use 220uF?

Regards,
Oba