Hi,
I am looking for a LDO for my customer to reduce the noise. Below is the requirements:
Vin,min < 2V
Vin,max > 5V
Vout,max >=4.4V
Vout,min < 1.2V
Output discharge
Iout(max) = 500mA
PSRR >= 70dB @ 1kHz
IQ(max): <= 20 uA (Not the most important, but the smaller the better.)
drop voltage <= 200mV @ 500mA
I think LP5912 is a choice. Could you please help check it or provide some other better choices? Thanks.