This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS767-Q1: output delay of 3.3V and 1.8V

Part Number: TPS767-Q1
Other Parts Discussed in Thread: DS90UB921-Q1EVM, TLV840-Q1, TPS767

Hi Expert,

I see TPS767D318PWP is used for supplying DS90UB921AS-Q1 in its reference design. You can see the TPS767D318PWP part as below. As required, the 3.3V cannot be applied earlier than 1.8V. In this design, I don't see the delay part. So how could it guarantee  3.3V will not be applied earlier than 1.8V, since the delay on circuit is random?

Thanks for your support!

BR, 

Elec Cheng