Hello team,
1. What is appropriate current limit range to set for TPS2H000-Q1? Is this 50mA to 900mA as specified in the CL accuracy? Does it mean appropriate R(CL) range should be 4.8kOHm - 267Ohm?
2. The abs max table shows "current on CL pin" is 6mA.
Does it mean R(CL) < 133Ohm cause the issue to the device?
Are there any other scenario that we should take care to comply this abs max?
Thanks.
Regards,
Hirata