Hi,
My customer measure fsw is around 800kHz. VIn=12V, Vout=3.3V.
According to datasheet, it shows fsw spec typical value at output voltage is 3.3V.
Could you please provide fsw spec at output voltage is 5V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer measure fsw is around 800kHz. VIn=12V, Vout=3.3V.
According to datasheet, it shows fsw spec typical value at output voltage is 3.3V.
Could you please provide fsw spec at output voltage is 5V?
Hi Jim,
The fsw selection and the spec provided are based on the resistor divider ratio as shown in Table 1, and it is independent of the output voltage.
Thank you,
Tomoya
Hi Ide,
Sorry, let me clarify my question again.
My question is my customer's hardware design is 600kHz, but the test result is about 800kHz.
Due to the fsw spec in datasheet is base on Vout=3.3V.
My customer design is Vout=5V so we should expect the fsw will be higher than 600kHz, am I correct?
If so, what's fsw spec for Vout=5V when fsw hardware design is 600kHz? Or do you have any simulation/test result can provide to my customer for reference?
Hi Gu,
Attached is customer's circuit. The divider is 249kohm on top and 107kohm on bottom
.
Hi Jim,
Have customers checked the actual resistance?
As Tomoya mentioned, the fsw selection provided are based on resistor divider ratio, which should be independent of output voltage.