Other Parts Discussed in Thread: TPS40210
Hello,
according this sheet, the fit rates for AEC-Q and non AEC-Q are the same, can you confirm, that there is no difference in fit rates for this two versions?
https://www.ti.com/lit/fs/slvaeu2/slvaeu2.pdf
According to the Datasheets, the soft-start offset voltage nominal value for AEC-Q version is typ 1 V, and for the non AEC-Q version it's 700 mV.
Is there a difference between this two versions and if yes, why?
According to the Datasheets, the ESD ratings are different, is this only because of the measurement standart (AEC Q vs JEDEC) or do they have different ratings?
Thanks for your answers.