Hi team,
I help my customer to post.
Problem Description of TPS56637 Application (1).docx
Thank you very much for your help.
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I help my customer to post.
Problem Description of TPS56637 Application (1).docx
Thank you very much for your help.
Best regards,
Hi Zhonghui,
According to the problem description, after removing TPS56637 chip, the positive and negative terminal (P31 1& 2 connecter) were shorted, if this is true, I highly suspected the input cap C1/C3/C4 may be shorted or mostly shorted. Can you double check the input cap status or replace new one? What's more, what is the input cap voltage rating, 25V/35V/...?
Thanks,
Lishuang
Hi Lishuang,
Min is my customer and the initiator of this problem. He knows the details very well.You can communicate with him directly.
Thanks.
Best regards,
Hi Min,
1. Have you done ABA swap test to confirm the unit was damaged? Seems you only did half of ABA swap test. Please also solder the 'damaged' chip onto a good board, to see whether the issue will happen.
2. From your description, the chip's Vin pin was short to ground? Could you measure all pins' impedance (to ground) of good chip v.s. damaged chip? Any other pins short to ground?
3. I found you use 2x22uF as Cout. Have you checked the 22uF cap derating ratio at 12V? Please make sure the actual Cout value is over 25uF, as suggested in datasheet Table 4.
Hi Min,
Sorry, I misunderstood the positive and negative terminals are for board.
Adding one comment based on Miranda's,
4. Which schematic or which inductor is the damaged chip used? L1 or L2? I found that L1 saturated current is only 3.5A while your application is 6A. If the L1 is saturated, the chip may be damaged. Would you mind to change a new inductor with higher current rating, higher than IOC max 8.6A would be good.
Thanks,
Lishuang
Thanks
MIN LI
Both circuits in the schematic have been tested, and both chips are broken. The reason why the rated current of the inductors is different is that Party A's project needs to verify whether the two inductors have the same characteristics and can be replaced (regardless of the current size).
Thanks
MIN LI
Hi Min,
Okay.
1. Can we understand that both circuits layout/components are same, except inductor? Both of them are damaged.
2. When does the damage happen? during power on or long time under 6A steady state?
3. Figure 1 shows it can be stable at 24Vin-12Vout-6A, can you help to measure the VIN SW Vout and inductor current waveforms during power on and steady state? If both of the new device with SCH1 and SCH2 can be only normal at 1A, would you mind to measure above waveforms under 1A under whistling?
4. I will double check the layout later. Now, our Allegro license server has some error, can't open the layout now.
Thanks,
Lishuang
According to your proposal, we added two 10uf aluminum electrolytic capacitors yesterday at the output end, and now the test chip is not broken. In turn, the output current was 1a,2a,3a,4a,5a,6a, and now the chip can be run properly and the chip is not broken. But there's a new little problem, which is that after the 6a long run, for example, the output voltage that runs 20 seconds will immediately fall and it will recover immediately(We recorded a video about this process), and we used the thermocouple thermometer to test the temperature of the chip shell at about 116 degrees Celsius. So we wonder if it is the internal heat of the chip triggers the heat protection in the inside of the chip? If that's the case, is there some good suggestion on Heat Dissipation about this chip.
According to your proposal, we added two 10uF/50V aluminum electrolytic capacitors yesterday at the output end, and now the test chip is not broken. In turn, the output current was 1a,2a,3a,4a,5a,6a, and now the chip can be run properly and the chip is not broken. But there's a new little problem, which is that after the 6a long run, for example, the output voltage that runs 20 seconds will immediately fall and it will recover immediately (We recorded a video about this process, this phenomenon occurred at 21s), and we used the thermocouple thermometer to test the temperature of the chip shell at about 116 degrees Celsius. So we wonder if it is the internal heat of the chip triggers the heat protection in the inside of the chip ? If that's the case, is there some good suggestion on Heat Dissipation about this chip.
Hi Min,
It's likely to trigger thermal shutdown. Please refer to datasheet page5.
You need to improve circuit efficiency (e.g. use a smaller DCR inductor) and improve your layout to better dissipate the heat.