Other Parts Discussed in Thread: TPS61170
Hi,
I like to compute the power dissipation of TPS61170 to ensure the temperature rise . (MOSFET and current sense resistors are embedded into the device). Could you please provide the formula and required data to compute. I am using this device for boost converter. Below are the data used in our boost converter, However, is it possible to give relation or variation with respect to output current ? Because, Vin and Vo will remain same but, there will be a change in Io in future.
Vin : Min=5V; Typ=6V; Max=7V
Vo : Min=11V; Typ=12V; Max=13V
Io : 150mA Max
Thanks,
Hema