This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
How can an implementation of parallel load switches with common outputs be configured to remove issue of reverse body diode currents?
Please find example block diagram of configuration below.
Issue would be if Vin 1 or 2 is supplying current while the other input is off. Then the body diode will saturate and source the second input.
KR,
Lucas
Hello Lucas,
In order to use load switches to power mux you'll need to use devices with reverse current protection such as TPS22916, TPS22917, TPS22948, etc. I've linked the product folder below with RCP device filter.
There are two types of reverse current protection. One type is always enabled, and the other is enabled when the device is disabled (ON pin low for active high devices). The second link provided will explain in more detail how to use load switches to power mux.
Power Multiplexing with Load Switches
Regards,
Kalin Burnside